MEDICAL
Digital X-Ray
Digital X-ray machines utilize a combination of digital image processing and X-radiation technologies to generate radiographs. They are equipped with X-ray detectors which replace traditional plastic films to produce digitalized images. Compared with the legacy equipments, digital X-ray machines realize a faster imaging process with better quality, and more importantly, reduce radiation dose that is required for imaging.
Digital X-ray machines commonly use direct or indirect-conversion-based FPDs (Flat Panel Detectors) to detect X rays. A direct-conversion-based FPD, which converts received X rays into electric signals directly, is made up of an amorphous selenium layer and a TFT array. While an indirect-conversion-based FPD is built with an amorphous silicon layer, a photodiode array and a TFT array are used to convert X rays into visible light first with an amorphous silicon layer, and then convert into electric signals with a photodiode array.
A processor is used to control bias voltage imposed on TFT array, and also transmit the charge stored in TFT to a signal acquisition circuit according to a specific sequence by multiplexing. The signal acquisition circuit has an analog front end to convert the charge into voltage and amplify the voltage which represents power level of X-ray. The amplified signal is converted to digital signal by an A/D converter, and then processed by a DSP to create images. These images could be displayed on screen, printed or transmitted to a remote terminal for medical diagnosis.
With the introduction of new materials to FPDs and the development of digital image processing technology, digital X-ray machines with higher resolution and faster and more accurate image reconstruction are set to replace traditional X-ray devices.
Hover over the diagram blocks to view recommended products for this solution:
DSP with high performance used to implement image processing
Click for full parts list
FPGA with high performance used to implement image processing
Click for full parts list
High performance MCU/MPU with multiple I/Os is required
Click for full parts list
High resolution, high SNR ADC is required
Click for full parts list
High resolution, DAC is required
Click for full parts list
Low noise, high precise amplifier is required
Click for full parts list
It is used to implement high-speed serial communications with the image processing unit
Click for full parts list
Touch Screen Controller
Power Management
Click for full parts list
Voltage Reference
Click for full parts list
LCD - Display
Click for full parts list